i.MX6 Quad reset time in serial downloader mode when WDOG_ENABLE=1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 Quad reset time in serial downloader mode when WDOG_ENABLE=1

Jump to solution
1,732 Views
m_c
Senior Contributor I

In figure 8-2 USB Boot Flow of IMX6DQRM Rev. 2, it said ARM core will reset if no any activity within 32 seconds when WDOG_ENABLE=1. However, in ERR006282 of IMX6DQCEC Rev. 4. The workaround #2 said, the Watchdog timer begins a 90-second countdown and, if nothing interrupts this process, the part resets.

1. The 32 and 90 seconds. Which one is right?

2. Is this delay time can change or not?

Labels (2)
0 Kudos
Reply
1 Solution
1,483 Views
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

1. 90sec

2. yes, from sect.70.5.1.1 IMX6DQRM  :

..The timeout value can be changed at any point..

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,484 Views
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

1. 90sec

2. yes, from sect.70.5.1.1 IMX6DQRM  :

..The timeout value can be changed at any point..

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,483 Views
m_c
Senior Contributor I

Is this timeout value will remain after cold reboot (power off, then power on)?

0 Kudos
Reply