i.MX6 Quad maximum ecspi clock rate (How to select suitable flash memory for the processor ? )

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6 Quad maximum ecspi clock rate (How to select suitable flash memory for the processor ? )

1,647 次查看
peteramond
Contributor V

Hi All,

Can we use a flash memory which has 104MHz supporting frequency (Device support high performance command for this frequency) with imax6 quad processor. Manufacturer part number - SST26VF032B-104I/MF

In imax6 DQIEC it has mentioned following under the ECSPI. So what is the maximum supporting frequency for ecspi clock ? What we should look for when we select flash memory for imax6 quad processor ?

pastedImage_1.png

Regards,

Peter.

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

1,498 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  please look at the following FAQ :

https://community.nxp.com/docs/DOC-95461 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复