i.MX6: Problem on the size of the partition after a formatting in FAT32 of a SDcard

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6: Problem on the size of the partition after a formatting in FAT32 of a SDcard

1,910 Views
gaylordlebrun
Contributor II

Hello to all,

Here is my situation, I possess a SDcard of 8 Go, when I take up it on my system, the only partition makes approximately 7.4 Go. But after I format (mkfs.vfat -I -F 32  /dev/<>p1) this partition is no more than of 2 Go.

How may I make for preserved the initial size?

Thank you in advance for any answers.

Best regards

Gaylord

Labels (2)
Tags (3)
0 Kudos
Reply
3 Replies

1,763 Views
b36401
NXP Employee
NXP Employee

I do not know what goes wrong in your case. I was unable to reproduce the issue.
Please try to omit "-I -F 32" they are not actually required but maybe they causes this issue somehow.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,763 Views
gaylordlebrun
Contributor II

Thanks Victor

But I try to omit "-I -F 32" and It is the same result, I have no more than 2Go of storage.

Best regards

Gaylord

0 Kudos
Reply

1,763 Views
yan2anfei
Contributor III

the fdisk has bug.

0 Kudos
Reply