i.MX6: Problem on the size of the partition after a formatting in FAT32 of a SDcard

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6: Problem on the size of the partition after a formatting in FAT32 of a SDcard

1,882 次查看
gaylordlebrun
Contributor II

Hello to all,

Here is my situation, I possess a SDcard of 8 Go, when I take up it on my system, the only partition makes approximately 7.4 Go. But after I format (mkfs.vfat -I -F 32  /dev/<>p1) this partition is no more than of 2 Go.

How may I make for preserved the initial size?

Thank you in advance for any answers.

Best regards

Gaylord

标签 (2)
标记 (3)
0 项奖励
回复
3 回复数

1,735 次查看
b36401
NXP Employee
NXP Employee

I do not know what goes wrong in your case. I was unable to reproduce the issue.
Please try to omit "-I -F 32" they are not actually required but maybe they causes this issue somehow.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,735 次查看
gaylordlebrun
Contributor II

Thanks Victor

But I try to omit "-I -F 32" and It is the same result, I have no more than 2Go of storage.

Best regards

Gaylord

0 项奖励
回复

1,735 次查看
yan2anfei
Contributor III

the fdisk has bug.

0 项奖励
回复