i.MX6 PCIe connection when JTAG debugger is used.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 PCIe connection when JTAG debugger is used.

Jump to solution
1,502 Views
satoshishimoda
Senior Contributor I

Hi community,

I want to confirm the connection of i.MX6 PCIe interface.

Please see the foot note of Table 2-21 in i.MX6 Hardware Development Guide (IMX6DQ6SDLHDG Rev.1).

It says "These supplies must remain powered if boundary scan test needs to be done".

Then, how about in a case that JTAG debugger is used even though JTAG boundary scan is not used?

Should I remain these supplies? or can I pull them down to GND?

Best Regards,

Satoshi Shimoda

Labels (5)
Tags (2)
0 Kudos
Reply
1 Solution
1,240 Views
LinWang
NXP Employee
NXP Employee

Hi Satoshi Shimoda,

The note doesn't impact JTAG debugger.

If there is no JTAG boundary scan required, you can follow both solutions.

Thanks!

View solution in original post

0 Kudos
Reply
2 Replies
1,241 Views
LinWang
NXP Employee
NXP Employee

Hi Satoshi Shimoda,

The note doesn't impact JTAG debugger.

If there is no JTAG boundary scan required, you can follow both solutions.

Thanks!

0 Kudos
Reply
1,240 Views
satoshishimoda
Senior Contributor I

Hi LinWnag,

Thank you for your prompt reply.

> If there is no JTAG boundary scan required, you can follow both solutions.

It's fine. Thank you!

Best Regards,

Satoshi Shimoda

0 Kudos
Reply