i.MX6 ODT Setting.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,161件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6DQ ODT.

Please see IOMUXC_SW_PAD_CTL_GRP_TERM_CTLx register in IMX6DQRM Rev.1.

These registers have "ODT" fields to determine the ODT values.

On the other hand, please see MMDCx_MPODTCTRL register (chapter 44.12.38).

These have "ODTx_INT_RES" fields to determine the ODT values, also.

Then, which registers have a priority to setting ODT value?

According to the following comment in IMX6D ODT, I guess MMDCx_MPODTCTRL have a priority, is this correct?

"3.  It is recommended to use only MMDC_MPODTCTRL register to configure ODT of i.MX6."

Best Regards,

Satoshi Shimoda

ラベル(4)
タグ(2)
0 件の賞賛
返信
1 解決策
1,757件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi,

these registers are working independently from each other (no priority).

And yes:

"3.  It is recommended to use only MMDC_MPODTCTRL register to configure ODT of i.MX6."

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,758件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi,

these registers are working independently from each other (no priority).

And yes:

"3.  It is recommended to use only MMDC_MPODTCTRL register to configure ODT of i.MX6."

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信