i.MX6 GPIO pull up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,688件の閲覧回数
sugiyamatoshihi
Contributor V

Hi,

I have a question pin output setting.

When a port is  output mode, it means OBE is enabled or functional output, is it possible to enable keeper or pull up/down resistor? 

In application note, AN5078, there is a description below.

The keeper device is able to keep the previous output value when the output driver is disabled.

Best Regards,

Sugiyama

ラベル(2)
0 件の賞賛
返信
1 解決策
2,426件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

I apologize, but I do not understand what you want to your question.  However, if you want to know if it is possible to enable/disable the keeper. Yes, it is possible.

Best Regards,

Diego.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,427件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

I apologize, but I do not understand what you want to your question.  However, if you want to know if it is possible to enable/disable the keeper. Yes, it is possible.

Best Regards,

Diego.

0 件の賞賛
返信
2,426件の閲覧回数
sugiyamatoshihi
Contributor V

Hi, Diego,

Thank you for the answer.

I also think it is strange. I asked customer why pullup/down is required in output mode, but no answer, yet.

Anyway, I understand pullup/down  and keeper can enable regardless input and output mode.

Best Regards,

Sugiyama

0 件の賞賛
返信