Hi community,
I have a question about i.MX6 DDR3 caliblation (ddr_stress_tester_v2.40).
I'd like to calculate the actual delay of
DG_DL_ABS_OFFSET0,WL_DL_ABS_OFFSET0,RD_DL_ABS_OFFSET0 and WR_DL_ABS_OFFSET0.
So,I used ddr_stress_tester_uboot_v2.40 with our custom mx6Q board.
And,I got the following result.
**result**
WL_DL_ABS_OFFSET0:0x23
DG_DL_ABS_OFFSET0:0x334
RD_DL_ABS_OFFSET0:0x5A
WR_DL_ABS_OFFSET0:0x34
************
While,
ARM core speed :1GHz (1.0ns)
DDR_CLK frequency: 528MHz (1.894ns)
When I calculate the value of DG_DL_ABS_OFFSET0 etc. ,
which value should I choose out of 1GHz,528MHz or other frequency ?
According to *"i.MX 6Dual/6Quad Applications Processor Reference Manual,
Rev. 2, 06/2014"(*page 3977).
The following sentence exists.
"The delay of the delay-line would be (DG_DL_ABS_OFFSET0 / 256)* MMDC_CH0
AXI clock (fast clock)."
What is the value of "MMDC_CH0 AXI clock(fast clock) " ?
I think it is 528MHz.
Is this correct or not ?
Likewise,what is the value of "clock period" of "WL_DL_ABS_OFFSET0" ?
Best Regards,
Seiichi Nakano
Hello,
Yes, by default it is 528 Mhz. Please use Figure 18-2 ( Clock Tree - Part 1)
of the i.MX6 RM regarding MMDC_CH0_CLK_ROOT and MMDC_CH1_CLK_ROOT.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello yuri
Thank you very much for your answer.
but,I have two additional questions.
((First question))
According to "i.MX 6Dual/6Quad Applications Processor Reference Manual, Rev. 2, 06/2014"(page 3865).
The following sentence exists.
"Under best-case conditions, -40C, 1.21V - 1.6ns."
In this situation(Under best case),
what is the value of "MMDC_CH0 AXI clock(fast clock) " ?
IF MMDC_CH0 AXI clock equal to 528MHz,
the maximum delay should be about 0.947ns( half cycle of 528MHz).
((Second question))
Is the CLK for "WL_DL_ABS_OFFSET0" also 528MHz?
In MPWLDECTRL0 field descriptions, I couldn't find "MMDC_CH0 AXI clock(fast clock)" ,only "clock period" exists.
Best Regards,
Seiichi Nakano
hello
Now I'm going to reply.
************************************
I understood about below.
1.The best-case and worst-case conditions,, relate to internal delays
(gates), and are not frequency dependent.
2."WL_DL_ABS_OFFSET0" is memory clock. Usually it is 528 MHz.
************************************
Thanks you.
2016-03-07 14:24 GMT+09:00 Yuri <admin@community.freescale.com>:
NXP Community
<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
i.MX6 DDR3 caliblation: How to calculate the value of DG_DL_ABS_OFFSET0
etc.
reply from Yuri Muhin
<https://community.freescale.com/people/Yuri?et=watches.email.thread> in *i.MX
Community* - View the full discussion
<https://community.freescale.com/message/621894?et=watches.email.thread#comment-621894>
Page 3747 of reference manual IMX6DQRM says:
WL_DL_ABS_OFFSET0 Absolute write-leveling delay offset for Byte 0. This field indicates the absolute delay between CK and write DQS of Byte0 with fractions of a clock period and up to half cycle. This value is process and frequency independent. The value of the delay can be calculated using the following equation (WR_DL_ABS_OFFSET1 / 256) * clock period
why here WR_DL_ABS_OFFSET1 is used in formula why not WR_DL_ABS_OFFSET0?