i.MX6 Boot from SPI - alternative pinmux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 Boot from SPI - alternative pinmux

Jump to solution
1,643 Views
dmitryv
Contributor II

Hello!

I have a question regarding iMX6 boot from SPI flash. If you look to MCIMX6Q-SDB schematics, you will find the following pin connection for SPI NOR flash (only 2 lines as example):

  SPINOR_CLK  --->>> KEY_COL0 [W5] . ALT0 = ECSPI1_CLK

  SPINOR_MISO --->>> KEY_COL1 [U7] . ALT0 = ECSPI1_MISO

However, according to RM "Table 8-25. SPI IOMUX Pin Configuration", or DS "Boot Devices Interfaces Allocation", booting from ECSPI1 is possible if connected to EIM_D17.alt1, EIM_D18.alt1, etc...

Does that mean that MCIMX6Q-SDB is not able to boot from onboard SPI NOR flash?

Or does boot ROM look to alternative pin options as well?

Thank you!

--

Dmitry

Labels (1)
0 Kudos
Reply
1 Solution
1,225 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dmitry

you are correct:

from i.MX_6Dual6Quad_SABRE-SD_Linux_Release_Notes.pdf L3.0.35_4.1.0_LINUX_DOCS

Table 7. Known Issues and Workarounds

"Current SD board uses KEY relative PINs as

SPI interface. However, this set of PINs are not

supported by ROM.

Therefore, SPI NOR boot is not supported by Smart Device Board."

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,226 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dmitry

you are correct:

from i.MX_6Dual6Quad_SABRE-SD_Linux_Release_Notes.pdf L3.0.35_4.1.0_LINUX_DOCS

Table 7. Known Issues and Workarounds

"Current SD board uses KEY relative PINs as

SPI interface. However, this set of PINs are not

supported by ROM.

Therefore, SPI NOR boot is not supported by Smart Device Board."

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply