Wondering if there is an issue with the i.MX6Q SPI. ...

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Wondering if there is an issue with the i.MX6Q SPI. ...

993 次查看
ScottKerstein
Contributor III

Looking into an issue with SPI and are trying to determine if we have an issue inside our mid-level driver, which we suspect, or if something else is going on. I am wondering if you have seen any issues with the SPI on the i.MX6, specifically anything with the slave strobe on read and write. I am looking for errata information or any known issues with the Linux 3.0.35 reference design. I am trying to eliminate anything from the silicon up to our mid-level driver as an issue. Any information you can provide would be helpful.

标签 (3)
0 项奖励
回复
1 回复

848 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Scott

there are no silicon issues with i.MX6Q eCSPI, just for reference example

and errata document IMX6DQCE

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复