i.MX6 Android BSP HWcomposer error.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 Android BSP HWcomposer error.

Jump to solution
5,477 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6DQ Android BSP (jb4.2.2_1.0.0).

Our partner tried to switching a screen from Android application, but it was failed with the following error which is output by /device/fsl-proprietary/gpu-viv/lib/hw/hwcomposer_viv.imx6.so.

=====

E/v_hwc   ( 2259): Failed in _ClearWormHole: status=-1

E/v_hwc   ( 2259): Failed in hwcComposeG2D: status=-1

E/v_hwc   ( 2259): _Set(939): Compose failed

E/v_hwc   ( 2259): Failed in _ClearWormHole: status=-1

E/v_hwc   ( 2259): Failed in hwcComposeG2D: status=-1

E/v_hwc   ( 2259): _Set(939): Compose failed[[359]]54'10"279 522

E/v_hwc   ( 2259): Failed in _ClearWormHole: status=-1

E/v_hwc   ( 2259): Failed in hwcComposeG2D: status=-1

E/v_hwc   ( 2259): _Set(939): Compose failed

E/v_hwc   ( 2259): Failed in _ClearWormHole: status=-1

E/v_hwc   ( 2259): Failed in hwcComposeG2D: status=-1

E/v_hwc   ( 2259): _Set(939): Compose failed

E/v_hwc   ( 2259): Failed in _ClearWormHole: status=-1

E/v_hwc   ( 2259): Failed in hwcComposeG2D: status=-1

E/v_hwc   ( 2259): _Set(939): Compose failed

=====

[Question]

Could you let me know what case is the above error output?

What should we do to resolve this issue?

Best Regards,

Satoshi Shimoda

Labels (3)
Tags (3)
0 Kudos
Reply
1 Solution
4,243 Views
ChucoChe
NXP Employee
NXP Employee

Clipping was added to make sure the coordinates were valid on the screen.

That change is included in jb4.3 and in the next release.

Michel

View solution in original post

0 Kudos
Reply
10 Replies
4,243 Views
satoshishimoda
Senior Contributor I

Could you reply to me anybody?

0 Kudos
Reply
4,243 Views
karina_valencia
NXP Apps Support
NXP Apps Support
Re: Re: i.MX6 Android BSP HWcomposer error.

Guillermo Michel JimenezEmployee

Hi,

Sorry for the delay. Could you try the attached SO?

Michel

0 Kudos
Reply
4,243 Views
satoshishimoda
Senior Contributor I

Hi Karina Valencia Aguilar,

Unfortunately, I could not download the .so file even though I clicked the link with a "Unauthorized" message.

Could you send me it again?

Best Regards,

Satoshi Shimoda

0 Kudos
Reply
4,242 Views
ChucoChe
NXP Employee
NXP Employee

Here it is.

Michel

4,242 Views
satoshishimoda
Senior Contributor I

Hi Michel,

We have two questions about the library you sent me.

Q1.

What is modified?

Q2.

Does Android 4.2.2_1.1.0 BSP include this library?

Best Regards,

Satoshi Shimdoa

0 Kudos
Reply
4,244 Views
ChucoChe
NXP Employee
NXP Employee

Clipping was added to make sure the coordinates were valid on the screen.

That change is included in jb4.3 and in the next release.

Michel

0 Kudos
Reply
4,242 Views
satoshishimoda
Senior Contributor I

Hi Michel,

Thank you for your reply, but sorry I did not understand what is "clipping".

Could you kindly let me know what is it?

And what is "next release"?

Next release of android 4.2.2? or next release of jb4.3?

If it means next release of jb4.3, does the library work well on jb4.2 even though android version is not same?

Best Regards,

Satoshi Shimoda

0 Kudos
Reply
4,242 Views
ChucoChe
NXP Employee
NXP Employee

Clipping means that only the a valid rectangle is switched to the other screen, by "clipping" what is not valid.

The change will be available in jb4.3 and there should be no problem in using the SO provided in this thread since it comes from the same source three.

Just keep in mind the change hasn't been extensively tested, just unittested. It will be extensively tested in jb4.3.

Michel

4,242 Views
denniswang_tw
Contributor II

Hi Michel,

I have another hwcomposer issue at below thread.

imx6DL dual display - hwcomposer_viv.imx6.so crash

My environment is 4.4.2 and upgrade to android_kk4.4.2_1.0.0-ga_core_source.tar.gz already.

This issue was gone after update your hwcomposer_viv.imx6.so.zip

Is any official release for this library? release note?

Where I can get newest release for 4.4.2?

Thanks.

0 Kudos
Reply
4,242 Views
satoshishimoda
Senior Contributor I

Hi Michel,

Thank you, I could download it.

And please wait a little to test the library.

Best Regards,
Satoshi Shimoda

0 Kudos
Reply