i.MX6 Android 4.4.2 audio HAL missing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 Android 4.4.2 audio HAL missing

1,782 Views
YanjunLuo
Contributor IV

I'm runing Android 4.4.2 on my own i.MX6Q, the sound codec I used STGL5000, now it works well with tinyalsa, I can play music and record sound. But I found there is no audio HAL inside the Android source code, there are no audio folder inside the hardware/imx/mx6 folder at all. Is there anything I missed or I need write an audio HAL from scratch?

Regards,

Yanjun Luo.

Labels (3)
0 Kudos
Reply
2 Replies

1,537 Views
SergioSolis
NXP Employee
NXP Employee

Hello Yanjun,

You can find it in the following path: myandroid/hardware/imx/alsa.



Best regards,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,537 Views
YanjunLuo
Contributor IV

Hi Sergio,

Thanks, I'm switch to another job now, I'll check it next week.

Regards,

Yanjun Luo.

0 Kudos
Reply