i.MX53 TZIC PRIORITY_MASK register setting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX53 TZIC PRIORITY_MASK register setting

ソリューションへジャンプ
1,808件の閲覧回数
torus1000
Contributor V

Hi chip experts,

I'm confusing about PRIORITY_MASK setting in TZIC of i.MX53.
I beleive highest priority is 0 but usage describe as following.

The ARM platform will

only receive an interrupt if there is a pending interrupt with a priority higher than the

value in this register. If an interrupt source asserts and its priority is equal to or lower

than the priority mask value, it will not cause an interrupt to the ARM platform.

Does "higher" mean (PRIORITYn < PRIORITY_MASK)?


Does "equal to or lower" mean (PRIORITYn >= PRIORITY_MASK)?

Can anyone clarify for me?

Thanks.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,737件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

I believe you are right, highest priority value is 0, as describes

below part of RM

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,738件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

I believe you are right, highest priority value is 0, as describes

below part of RM

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信