i.MX53 TZIC PRIORITY_MASK register setting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX53 TZIC PRIORITY_MASK register setting

Jump to solution
1,789 Views
torus1000
Contributor V

Hi chip experts,

I'm confusing about PRIORITY_MASK setting in TZIC of i.MX53.
I beleive highest priority is 0 but usage describe as following.

The ARM platform will

only receive an interrupt if there is a pending interrupt with a priority higher than the

value in this register. If an interrupt source asserts and its priority is equal to or lower

than the priority mask value, it will not cause an interrupt to the ARM platform.

Does "higher" mean (PRIORITYn < PRIORITY_MASK)?


Does "equal to or lower" mean (PRIORITYn >= PRIORITY_MASK)?

Can anyone clarify for me?

Thanks.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,718 Views
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

I believe you are right, highest priority value is 0, as describes

below part of RM

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,719 Views
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

I believe you are right, highest priority value is 0, as describes

below part of RM

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply