Hi chip experts,
I'm confusing about PRIORITY_MASK setting in TZIC of i.MX53.
I beleive highest priority is 0 but usage describe as following.
The ARM platform will
only receive an interrupt if there is a pending interrupt with a priority higher than the
value in this register. If an interrupt source asserts and its priority is equal to or lower
than the priority mask value, it will not cause an interrupt to the ARM platform.
Does "higher" mean (PRIORITYn < PRIORITY_MASK)?
Does "equal to or lower" mean (PRIORITYn >= PRIORITY_MASK)?
Can anyone clarify for me?
Thanks.