i.MX53 SSI Interface with Audio DAC WM8523 - Sampling Rate Issue:

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX53 SSI Interface with Audio DAC WM8523 - Sampling Rate Issue:

Jump to solution
3,136 Views
GopiNagaBharath
Contributor IV

Hi All,

We are using Audio DAC WM8523 from Wolfson in our i.mX53 based custom board.

The Audio DAC is interfaced to to the i.MX53 processor through I2S (Audio Mux) & I2C (Software Control Interface).

The WM8523 driver used is from (provided by Wolfson) : http://opensource.wolfsonmicro.com/cgi-bin/gitweb.cgi?p=linux-2.6-asoc.git;a=blob_plain;f=sound/soc/...

When we use this we are getting an error - "No MCLK configured, call set_sysclk() on init" and the System unable to detect the DAC as the sound device.

Has anyone used WM8523 with any of the i.MX series Processors and were able to get it work?

Regards,

Gopi

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,650 Views
GopiNagaBharath
Contributor IV

Yes, i have fixed the issue.

Thanks,

Gopi

View solution in original post

0 Kudos
Reply
3 Replies
2,650 Views
YixingKong
Senior Contributor IV

GopiNagaBharath

We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow to resolved the

issue, can we close the discussion? If you still need Freescale help, please feel free to contact us.

Thanks,
Yixing

0 Kudos
Reply
2,651 Views
GopiNagaBharath
Contributor IV

Yes, i have fixed the issue.

Thanks,

Gopi

0 Kudos
Reply
2,650 Views
YixingKong
Senior Contributor IV

Thanks, I will close the discussion.

Yixing

0 Kudos
Reply