i.MX53 SSI Interface with Audio DAC WM8523 - Sampling Rate Issue:

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX53 SSI Interface with Audio DAC WM8523 - Sampling Rate Issue:

ソリューションへジャンプ
3,116件の閲覧回数
GopiNagaBharath
Contributor IV

Hi All,

We are using Audio DAC WM8523 from Wolfson in our i.mX53 based custom board.

The Audio DAC is interfaced to to the i.MX53 processor through I2S (Audio Mux) & I2C (Software Control Interface).

The WM8523 driver used is from (provided by Wolfson) : http://opensource.wolfsonmicro.com/cgi-bin/gitweb.cgi?p=linux-2.6-asoc.git;a=blob_plain;f=sound/soc/...

When we use this we are getting an error - "No MCLK configured, call set_sysclk() on init" and the System unable to detect the DAC as the sound device.

Has anyone used WM8523 with any of the i.MX series Processors and were able to get it work?

Regards,

Gopi

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,630件の閲覧回数
GopiNagaBharath
Contributor IV

Yes, i have fixed the issue.

Thanks,

Gopi

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,630件の閲覧回数
YixingKong
Senior Contributor IV

GopiNagaBharath

We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow to resolved the

issue, can we close the discussion? If you still need Freescale help, please feel free to contact us.

Thanks,
Yixing

0 件の賞賛
返信
2,631件の閲覧回数
GopiNagaBharath
Contributor IV

Yes, i have fixed the issue.

Thanks,

Gopi

0 件の賞賛
返信
2,630件の閲覧回数
YixingKong
Senior Contributor IV

Thanks, I will close the discussion.

Yixing

0 件の賞賛
返信