i.MX502 power-up sequence

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX502 power-up sequence

Jump to solution
2,036 Views
norishinozaki
Contributor V

Hello,

I'm creating i.MX502 power-up sequence by referring to SDG and the EVK schematics.

I found 3.15V including VDD3P0 is supplied by DC/DC, not by MC34708.

Then it looks the DC/DC is enable by GPIO after the CPU core startups.

Is this correct?

pastedImage_3.png

In the case, the VDD3P0 is almost the last to be enabled

Are VDD2P5, VDD1P8, VDD1P2 Ok to be enabled before VDD3P0?

Best regards,

Nori Shinozaki

Labels (1)
0 Kudos
Reply
1 Solution
1,953 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nori

VDD2P5, VDD1P8, VDD1P2 should be enabled after VDD3P0

as shows Figure 2

Note there may be discrepancies between reference design and datasheet

descriptions since reference design is created before datasheet specs

are finalized.

Best regards

igor

View solution in original post

0 Kudos
Reply
4 Replies
1,953 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nori

some clarification is given at footnote 2

to IMX50CEC sect.4.2.1 Power-Up Sequence

2). No power-up sequence dependencies exist between the supplies shown

shaded in gray.

However VDD2P5, VDD1P8, VDD1P2 should be enabled after VDD3P0

as shows Figure 2

Note there may be discrepancies between reference design and datasheet

descriptions since reference design is created before datasheet specs

are finalized.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,953 Views
norishinozaki
Contributor V

Hello Igor,

I'm concerned on the following VDDs, not on the shaded ones

pastedImage_0.png

In the EVK, VDD2P5, 1P8, 1P2 are enabled prior to VDD3P0.

Regards,

Nori Shinozaki

0 Kudos
Reply
1,954 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nori

VDD2P5, VDD1P8, VDD1P2 should be enabled after VDD3P0

as shows Figure 2

Note there may be discrepancies between reference design and datasheet

descriptions since reference design is created before datasheet specs

are finalized.

Best regards

igor

0 Kudos
Reply
1,953 Views
norishinozaki
Contributor V

Igor,

I see, thank you!

Best regards,

Nori Shinozaki

0 Kudos
Reply