i.MX502 power-up sequence

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX502 power-up sequence

ソリューションへジャンプ
1,985件の閲覧回数
norishinozaki
Contributor V

Hello,

I'm creating i.MX502 power-up sequence by referring to SDG and the EVK schematics.

I found 3.15V including VDD3P0 is supplied by DC/DC, not by MC34708.

Then it looks the DC/DC is enable by GPIO after the CPU core startups.

Is this correct?

pastedImage_3.png

In the case, the VDD3P0 is almost the last to be enabled

Are VDD2P5, VDD1P8, VDD1P2 Ok to be enabled before VDD3P0?

Best regards,

Nori Shinozaki

ラベル(1)
0 件の賞賛
返信
1 解決策
1,902件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nori

VDD2P5, VDD1P8, VDD1P2 should be enabled after VDD3P0

as shows Figure 2

Note there may be discrepancies between reference design and datasheet

descriptions since reference design is created before datasheet specs

are finalized.

Best regards

igor

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,902件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nori

some clarification is given at footnote 2

to IMX50CEC sect.4.2.1 Power-Up Sequence

2). No power-up sequence dependencies exist between the supplies shown

shaded in gray.

However VDD2P5, VDD1P8, VDD1P2 should be enabled after VDD3P0

as shows Figure 2

Note there may be discrepancies between reference design and datasheet

descriptions since reference design is created before datasheet specs

are finalized.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,902件の閲覧回数
norishinozaki
Contributor V

Hello Igor,

I'm concerned on the following VDDs, not on the shaded ones

pastedImage_0.png

In the EVK, VDD2P5, 1P8, 1P2 are enabled prior to VDD3P0.

Regards,

Nori Shinozaki

0 件の賞賛
返信
1,903件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nori

VDD2P5, VDD1P8, VDD1P2 should be enabled after VDD3P0

as shows Figure 2

Note there may be discrepancies between reference design and datasheet

descriptions since reference design is created before datasheet specs

are finalized.

Best regards

igor

0 件の賞賛
返信
1,902件の閲覧回数
norishinozaki
Contributor V

Igor,

I see, thank you!

Best regards,

Nori Shinozaki

0 件の賞賛
返信