i.MX502 & MC34709 Power-down sequence

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX502 & MC34709 Power-down sequence

ソリューションへジャンプ
1,246件の閲覧回数
norishinozaki
Contributor V

Hello,

I'd like to use MC34709 PMIC along with i.MX502.

i.MX502 requires the power-off sequence in the reverse of the power-up.

In MC34709 datasheet, there is a power-up sequence for processors.

However there is no descriptions about the power-down sequence.

- What is the power-down sequence of MC34079?

- What will happen in i.MX502 if it's not power-down in the reverse of the power-up as instructed in the datasheet?

BTW i.MX503 can be powered down "Switch all supplies down simultaneously".

Best regards,

Nori Shinozaki

ラベル(1)
0 件の賞賛
返信
1 解決策
1,046件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nori

you are right that MC34079 datasheet has not descriptions

about the power-down sequence, that means that its supplies are

turned off simultaneously.

It was confirmed by app team that for i.MX50

basically, all power rails can be down at the same time.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
1,047件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nori

you are right that MC34079 datasheet has not descriptions

about the power-down sequence, that means that its supplies are

turned off simultaneously.

It was confirmed by app team that for i.MX50

basically, all power rails can be down at the same time.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,046件の閲覧回数
norishinozaki
Contributor V

Hello Igor,

You wrote "all power rails can be down at the same time."

I understood that there is no power-down sequence, NO need to shutdown all power rails at the same time.

My customer is just power-down at the same time, but actually the rails go down randomly.

In this case, they need to assert POR_B before beginning power-down.

Otherwise i.MX502 pins emit strange outputs during power-down.

Have you heard about this?

Is it OK with POR_B first then power rails go down randomly?

Best regards,

N.Shinozaki

0 件の賞賛
返信
1,046件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nori

yes it is ok with POR_B first then power rails go down randomly.

Best regards

igor

1,046件の閲覧回数
norishinozaki
Contributor V

Hello Igor,

Thanks!

N.Shinozaki

0 件の賞賛
返信
1,046件の閲覧回数
norishinozaki
Contributor V

Hello Igor,

Thank you!

Best regards,

Nori Shinozaki

0 件の賞賛
返信