Hello!
I have a problem with a custom i.MX287 board, based on Freescale EVK. It is using 5V only connection scheme with no battery present, and booting from an SD card. The same image is booting fine in EVK. Boot process goes fine until the Linux should boot up. Then the processor reboots endlessly. Debug data from DUART given below:
*************************************
PowerPrep start initialize power...
Configured for 5v only power source. Battery powered operation disabled.
LLLCJan 16 201315:05:46
FRAC 0x92925552
memory type is DDR2
Wait for ddr ready 1power 0x00820616
Frac 0x92925552
start change cpu freq
hbus 0x00000003
cpu 0x00010001
start test memory accress
ddr2 0x40000000
finish simple test
LLLLLLLFLCLLJ
*************************************
The next thing that should appear, is "Uncompressing Linux", but it never appears. The operating voltages seem to be at correct levels and stable.
Thanks in advance,
 Elias
Solved! Go to Solution.
 
					
				
		
 VladanJovanovic
		
			VladanJovanovic
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Are you using same DDR2 memory devices as on i.MX28EVK? If not, you will have to adjust memory controller setup sequence in the bootlets package.
Files to help with finding memory controller setup are here:
I downloaded the files you suggested. After correcting the memory bank count I have made progress. Now the kernel tries to boot:
LLLLLLLFLCLLJUncompressing Linux... done, booting the kernel.
Freescale OBDS boots to the following:
********************************************************
Diagnostics Suite (1.0) on i.MX28 evk
Build: Jan 25 2013, 10:32:42
Freescale Semiconductor, Inc.
********************************************************
---- Running < UART > test
Please enter y or Y to confirm
We are still not sure about those various parameters to do with the specific memory used.
The system is booting now. Thank you for your help!
We found the appropriate memory settings in this thread:
Re: Kernel execution stops at decompress function
regards,
Elias
 
					
				
		
You might be interested in checking U-Boot 2013.01 as it has full support to mx28evk; to adapt the code to your board shouldn't be hard and you can drop imx-bootlets.
 
					
				
		
 VladanJovanovic
		
			VladanJovanovic
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Are you using same DDR2 memory devices as on i.MX28EVK? If not, you will have to adjust memory controller setup sequence in the bootlets package.
Files to help with finding memory controller setup are here: