i.MX287 SD Card boot problem with a custom board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX287 SD Card boot problem with a custom board

ソリューションへジャンプ
2,545件の閲覧回数
overflow
Contributor I

Hello!

I have a problem with a custom i.MX287 board, based on Freescale EVK. It is using 5V only connection scheme with no battery present, and booting from an SD card. The same image is booting fine in EVK. Boot process goes fine until the Linux should boot up. Then the processor reboots endlessly. Debug data from DUART given below:

*************************************

PowerPrep start initialize power...

Configured for 5v only power source.            Battery powered operation disabled.

LLLCJan 16 201315:05:46

FRAC 0x92925552

memory type is DDR2

                    Wait for ddr ready 1power 0x00820616

Frac 0x92925552

start change cpu freq

hbus 0x00000003

cpu 0x00010001

start test memory accress

ddr2 0x40000000

finish simple test

LLLLLLLFLCLLJ

*************************************

The next thing that should appear, is "Uncompressing Linux", but it never appears. The operating voltages seem to be at correct levels and stable.

Thanks in advance,


Elias

ラベル(1)
0 件の賞賛
返信
1 解決策
1,801件の閲覧回数
VladanJovanovic
NXP Employee
NXP Employee

Are you using same DDR2 memory devices as on i.MX28EVK? If not, you will have to adjust memory controller setup sequence in the bootlets package.

Files to help with finding memory controller setup are here:

Memory controller setup for i.MX28 and i.MX50

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,801件の閲覧回数
overflow
Contributor I

I downloaded the files you suggested. After correcting the memory bank count I have made progress. Now the kernel tries to boot:

LLLLLLLFLCLLJUncompressing Linux... done, booting the kernel.

Freescale OBDS boots to the following:

********************************************************

     Diagnostics Suite (1.0) on i.MX28 evk

     Build: Jan 25 2013, 10:32:42

     Freescale Semiconductor, Inc.

********************************************************

---- Running < UART > test

Please enter y or Y to confirm

We are still not sure about those various parameters to do with the specific memory used.

0 件の賞賛
返信
1,801件の閲覧回数
overflow
Contributor I

The system is booting now. Thank you for your help!

We found the appropriate memory settings in this thread:

Re: Kernel execution stops at decompress function

regards,

Elias

0 件の賞賛
返信
1,801件の閲覧回数
OtavioSalvador
Senior Contributor II

You might be interested in checking U-Boot 2013.01 as it has full support to mx28evk; to adapt the code to your board shouldn't be hard and you can drop imx-bootlets.

0 件の賞賛
返信
1,802件の閲覧回数
VladanJovanovic
NXP Employee
NXP Employee

Are you using same DDR2 memory devices as on i.MX28EVK? If not, you will have to adjust memory controller setup sequence in the bootlets package.

Files to help with finding memory controller setup are here:

Memory controller setup for i.MX28 and i.MX50

0 件の賞賛
返信