i.MX28 EMAC and IP accelerator functions

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX28 EMAC and IP accelerator functions

883 次查看
stathisv
Contributor II

Hi all,

I am trying to enable IP header checksum insertion by the EMAC on the transmit path.

Although I set bit 3 (TX_IPCHK_INS) of register HW_ENET_MAC_IPACCTXCONF it does

not seem to have any effect. When I capture the packet with Wireshark the checksum

is still 0. Does this feature work in the legacy DMA mode?

I noticed that in the enhanced DMA mode this feature can be enabled via a control bit

on the DMA descriptor too.

Regards,

Stathis

标签 (1)
0 项奖励
回复
0 回复数