we are using imx258 as the main processor for a project. when tried to build modules in drivers/mxc/security, we met a lot of troubles. since could not find any resources in google, sincerely hope someone can give us answers to the following questions in this forum
1. should we use rng/shw_driver(.c) as our main tool to bridge user and kernel spaces programs?
2. scc2_driver can be used for imx258?
if the answer to this question is "NO", please, ignore the following 3 questions and jump to question 6 directly
3. if so, it is easy to see that some important functions such as shw_handle_scc_encrypt() and shw_handle_scc_decrypt() in shw_driver.c are totally useless if flag FSL_HAVE_SCC2 is not defined. since turning the FSL_HAVE_SCC2 on will call functions in scc2_driver.c, does this mean we must use scc2_driver.c?
4. there is an "old" version driver for scc (mxc_scc.c) having a lot functions also defined scc2_driver.c and this implies that they are mutually exclusive, doesn't it?
5. when we disabled FSL_HAVE_SCC and enabled FSL_HAVE_SCC2 we got trouble with "keystore" in fsl_shw_keystore.c. in mxc_scc.c key storage struct key_slot which is only applied in mxc_scc
6. finally, is the following function in dryice.c implemented correctly? it seems endless.
static void try_to_clear_wef(void)
{
int cnt;
while (1) {
di_write(DSR_WEF, DSR);
for (cnt = 0; cnt < DI_WRITE_LOOP_CNT; cnt++) {
if ((di_read(DSR) & DSR_WEF) == 0)
break;
}
di_warn("WARNING: DryIce cannot clear DSR_WEF "
"(Write Error Flag)!\n");
}
}