i.MX25: Unit in WEIM parameters

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX25: Unit in WEIM parameters

1,331 Views
norishinozaki
Contributor V

Hello Champs,

I'd like to get WE31 from a table from i.MX25 datasheet below

pastedImage_0.png

My CSA is 2, which equals to 1 BCLK = 125MHz = 8ns.

The Max value becomes -5ns.

Is this correct understanding?

Best regards,

Nori Shinozaki

Labels (1)
0 Kudos
Reply
3 Replies

1,239 Views
Yuri
NXP Employee
NXP Employee

  Your understanding is correct . CS is asserted later than address.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,239 Views
norishinozaki
Contributor V

Hello Yuri,

You mean WE4-WE6-CSA is correct and the MAX 3-CSA = -5ns is also correct value?

Best regards,

Nori Shinozaki

0 Kudos
Reply

1,239 Views
Yuri
NXP Employee
NXP Employee

yes.

0 Kudos
Reply