i.MX25 NAND, Boot Question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX25 NAND, Boot Question

3,974件の閲覧回数
jwsawyer
Contributor I

We would like to use a Micron MT29F1G08ABAEAWP NAND Flash memory device.with the i.MX25.

The Micron NAND x8 device is organized using a 2048 page size plus 64 spare bytes.

We are using these settings:

BT_PAGE_SIZE = 01 (2K)

BT_BUS_WIDTH = 00 (8b)

BT_MLS_SEL = 0 (SLC)

BT_SPARE_SIZE = 0

BT_MEM_CTRL = 01 (NAND)

BT_MEM_TYPE = 10 (5 address cycles)

We think this memory should work with the i.MX25.  It does have this cryptic note in the datasheet:

    Minimum required ECC for block 0 if PROGRAM/ERASE cycles are less than 1000  :  1-bit ECC per 528 bytes

Would you agree that this device should be compatible with the i.MX25 boot sequence and NFC operations?

If yes, we don't see the i.MX25 boot sequence send the 0x30 command for the READ PAGE command, so the NAND does not output data.

Thank you!

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

3,804件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi John

this part has 4-bit ECC and can be supported by i.MX25 as described

in sect.2.5 MLC/SLC NAND Devices AN3684 i.MX25 Boot Options

https://www.nxp.com/docs/en/application-note/AN3684.pdf 

For programming nand boot image recommended to use ATK Tool

(it correctly handles nand bad block management) as shown in attached documents

i.MX25 PDK Board Flashing SPI NOR 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,804件の閲覧回数
jwsawyer
Contributor I

Update - hardware folks found an issue with the Boot-Related pins.  Once corrected, we see the expected READ PAGE operation succeed on boot.

BUT...we are still having problems with reading data out of the device using NFC commands.  The read halts after 512 (maybe 528?) bytes, as REn stops being toggled by the micro.  But CEn remains low, so the INT pin never indicates that the read is complete.

RCSR = 0x64000900  [NFC_FMS = 1, NFC_4K = 0, MEM_CTRL = 1, MEM_TYPE = 2, PAGE_SIZE = 1, BUS_WIDTH = 0]

NAND_FLASH_CONFIG1 = 0x0A0B

Any suggestions?

Thanks again.

0 件の賞賛
返信