[i.MX1176] Is it possible to select 3.3V for ADC vref?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

[i.MX1176] Is it possible to select 3.3V for ADC vref?

跳至解决方案
2,115 次查看
kenji
Contributor IV

Hi Team

 

Is it possible to select 3.3V for ADC vref, with i.MX1176?
At maximum supply current, ADC_VREF condition seems like 3.3V.

I suppose that it will not be possible, but please tell me how use ADC_VREF 3.3V in case possible.

 

kenji_0-1637142488525.png

kenji_1-1637142639607.png

 

 

标记 (2)
0 项奖励
回复
1 解答
2,109 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Kenji,

You are correct in that the maximum voltage for VREFH would be 1.8V typical (1.89V absolute maximum).

However, you may use the full scale of the ADC in 3.3V mode by using the Channel Scale (ADCxCMDLy[CSCALE]) feature. This allows the input voltage to be higher than the reference.

You may find more details in section 87.6.1.3 and the ADCxCMDLy register section of the i.MXRT1170 Reference Manual (link below, please note that you may need to login to download this document).

https://www.nxp.com/webapp/Download?colCode=IMXRT1170RM

I hope that this information helps. Please let me know if there’s anything else that I can do for you.

Regards,
Gustavo

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,110 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Kenji,

You are correct in that the maximum voltage for VREFH would be 1.8V typical (1.89V absolute maximum).

However, you may use the full scale of the ADC in 3.3V mode by using the Channel Scale (ADCxCMDLy[CSCALE]) feature. This allows the input voltage to be higher than the reference.

You may find more details in section 87.6.1.3 and the ADCxCMDLy register section of the i.MXRT1170 Reference Manual (link below, please note that you may need to login to download this document).

https://www.nxp.com/webapp/Download?colCode=IMXRT1170RM

I hope that this information helps. Please let me know if there’s anything else that I can do for you.

Regards,
Gustavo

0 项奖励
回复
2,101 次查看
kenji
Contributor IV

Hi @gusarambula -san

Thank you!

0 项奖励
回复