[i.MX1176] Is it possible to select 3.3V for ADC vref?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[i.MX1176] Is it possible to select 3.3V for ADC vref?

Jump to solution
2,140 Views
kenji
Contributor IV

Hi Team

 

Is it possible to select 3.3V for ADC vref, with i.MX1176?
At maximum supply current, ADC_VREF condition seems like 3.3V.

I suppose that it will not be possible, but please tell me how use ADC_VREF 3.3V in case possible.

 

kenji_0-1637142488525.png

kenji_1-1637142639607.png

 

 

Tags (2)
0 Kudos
Reply
1 Solution
2,134 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Kenji,

You are correct in that the maximum voltage for VREFH would be 1.8V typical (1.89V absolute maximum).

However, you may use the full scale of the ADC in 3.3V mode by using the Channel Scale (ADCxCMDLy[CSCALE]) feature. This allows the input voltage to be higher than the reference.

You may find more details in section 87.6.1.3 and the ADCxCMDLy register section of the i.MXRT1170 Reference Manual (link below, please note that you may need to login to download this document).

https://www.nxp.com/webapp/Download?colCode=IMXRT1170RM

I hope that this information helps. Please let me know if there’s anything else that I can do for you.

Regards,
Gustavo

View solution in original post

0 Kudos
Reply
2 Replies
2,135 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Kenji,

You are correct in that the maximum voltage for VREFH would be 1.8V typical (1.89V absolute maximum).

However, you may use the full scale of the ADC in 3.3V mode by using the Channel Scale (ADCxCMDLy[CSCALE]) feature. This allows the input voltage to be higher than the reference.

You may find more details in section 87.6.1.3 and the ADCxCMDLy register section of the i.MXRT1170 Reference Manual (link below, please note that you may need to login to download this document).

https://www.nxp.com/webapp/Download?colCode=IMXRT1170RM

I hope that this information helps. Please let me know if there’s anything else that I can do for you.

Regards,
Gustavo

0 Kudos
Reply
2,126 Views
kenji
Contributor IV

Hi @gusarambula -san

Thank you!

0 Kudos
Reply