i.MX Linux compilation problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Linux compilation problem

ソリューションへジャンプ
3,514件の閲覧回数
pengjing918
Contributor II

1. Does the NXP i.MX series SOC only use yocto to compile and package the kernel, uboot, root file system?

2. Is there a separate BSP patch for Linux, and then add the BSP patch for i.MX to the Linux source code, and then compile it?

1.请问NXP i.MX系列SOC, 都只能使用yocto编译打包内核, uboot, 根文件系统吗? 

2.有没有单独提供Linux 的BSP补丁, 然后对Linux源码加上i.MX 的BSP补丁, 再编译的呢?

ラベル(7)
タグ(2)
1 解決策
3,309件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

1\Yes, the linux BSP use the Yocto.

2\Sorry, no this kind of patch.

I have searched one thread also use Yocto, but Standalone, hope it can do some for you.

Detailed Operations For Standalone On Linux BSP of I.MX Processors 

Have a nice day

Rita

元の投稿で解決策を見る

3 返答(返信)
3,310件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

1\Yes, the linux BSP use the Yocto.

2\Sorry, no this kind of patch.

I have searched one thread also use Yocto, but Standalone, hope it can do some for you.

Detailed Operations For Standalone On Linux BSP of I.MX Processors 

Have a nice day

Rita

3,309件の閲覧回数
pengjing918
Contributor II

Thank you very much for your answer.
Are you an employee of nxp?

0 件の賞賛
返信
3,309件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

You are welcome. Yes, many engineers in this community, you can create thread if you have questions.

0 件の賞賛
返信