i.MX Linux compilation problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Linux compilation problem

Jump to solution
3,588 Views
pengjing918
Contributor II

1. Does the NXP i.MX series SOC only use yocto to compile and package the kernel, uboot, root file system?

2. Is there a separate BSP patch for Linux, and then add the BSP patch for i.MX to the Linux source code, and then compile it?

1.请问NXP i.MX系列SOC, 都只能使用yocto编译打包内核, uboot, 根文件系统吗? 

2.有没有单独提供Linux 的BSP补丁, 然后对Linux源码加上i.MX 的BSP补丁, 再编译的呢?

Tags (2)
1 Solution
3,383 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

1\Yes, the linux BSP use the Yocto.

2\Sorry, no this kind of patch.

I have searched one thread also use Yocto, but Standalone, hope it can do some for you.

Detailed Operations For Standalone On Linux BSP of I.MX Processors 

Have a nice day

Rita

View solution in original post

3 Replies
3,384 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

1\Yes, the linux BSP use the Yocto.

2\Sorry, no this kind of patch.

I have searched one thread also use Yocto, but Standalone, hope it can do some for you.

Detailed Operations For Standalone On Linux BSP of I.MX Processors 

Have a nice day

Rita

3,383 Views
pengjing918
Contributor II

Thank you very much for your answer.
Are you an employee of nxp?

0 Kudos
Reply
3,383 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

You are welcome. Yes, many engineers in this community, you can create thread if you have questions.

0 Kudos
Reply