i.MX IOMUX when device tree does not set its function.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX IOMUX when device tree does not set its function.

ソリューションへジャンプ
1,739件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX Linux BSP.
I want to know what IOMUX is selected if I don't set it by device tree.
Is the initial setting written in datasheet selected?
(e.g. For i.MX6UL CSI_DATA00 pad, is CSI_DATA00 selected as datasheet Table 95 if no function is set by device tree?)


Best Regards,
Satoshi Shimoda

タグ(2)
0 件の賞賛
返信
1 解決策
1,601件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

>I want to know what IOMUX is selected if I don't set it by device tree.

IOMUX has settings left from uboot.

If uboot does not set them, then left from chip reset settings,

"initial setting written in datasheet selected".

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,602件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

>I want to know what IOMUX is selected if I don't set it by device tree.

IOMUX has settings left from uboot.

If uboot does not set them, then left from chip reset settings,

"initial setting written in datasheet selected".

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信