SIM Interface in iMX6UL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SIM Interface in iMX6UL

1,440件の閲覧回数
riteshpatel
Contributor II

Hi,

 

I am bit confuse about SIM interface on iMX6UL. 

 

As per technical reference manual page # 2799, "The SIM module has one port that can be used to interface with the various cards."  But block diagram shows two port, 0 & 1.

162460_162460.pngpastedImage_1.png

 

Referred i.MX6UL pin muxing, Found that there are four ports.

SIM1.Port0,

SIM1.Port1,

SIM2.Port0,

SIM2.Port1.

 

 

Will appreciate any help or clarification for understanding above with reference if any.

Can you please let me know on which two SIM ports i can connect smart card? As datasheet shows upto 2 SIM interface support.

Thanks,

Ritesh

ラベル(1)
0 件の賞賛
返信
1 返信

1,217件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to https://community.nxp.com/thread/434369 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信