i.MX IOMUX when device tree does not set its function.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX IOMUX when device tree does not set its function.

Jump to solution
1,734 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX Linux BSP.
I want to know what IOMUX is selected if I don't set it by device tree.
Is the initial setting written in datasheet selected?
(e.g. For i.MX6UL CSI_DATA00 pad, is CSI_DATA00 selected as datasheet Table 95 if no function is set by device tree?)


Best Regards,
Satoshi Shimoda

Tags (2)
0 Kudos
Reply
1 Solution
1,596 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

>I want to know what IOMUX is selected if I don't set it by device tree.

IOMUX has settings left from uboot.

If uboot does not set them, then left from chip reset settings,

"initial setting written in datasheet selected".

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,597 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

>I want to know what IOMUX is selected if I don't set it by device tree.

IOMUX has settings left from uboot.

If uboot does not set them, then left from chip reset settings,

"initial setting written in datasheet selected".

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply