i.MX 8M Mini galcore error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8M Mini galcore error

2,610 Views
jianfeichang
Contributor IV

问题一:开机卡死,log如下

Mounting Temporary Directory (/tmp)...
[ OK ] Listening on udev Control Socket.
Starting udev Coldplug all Devices...
Starting Load Kernel Modules...
[ 4.248055] galcore: loading out-of-tree module taints kernel.
[ 4.257498] galcore: clk_get vg clock failed, disable vg!
[ 4.263217] Galcore version 6.2.4.190076
[ OK ] Listening on /dev/initctl Compatibility Named Pipe.
[ 4.288498] Unable to handle kernel NULL pointer dereference at virtual address 00000008

一直停在这里,我用的是4.14.98官方的案例镜像,烧写到emmc,提示galcore卡死。

问题二:将官方的程序烧写到SD卡,提示

[ 3.515170] ALSA device list:
[ 3.518154] #0: wm8524-audio
[ 3.521218] #1: imx-spdif
[ 3.524024] #2: imx-audio-micfil
[ 3.527635] Waiting for root device /dev/mmcblk1p2...
[ 4.686635] random: crng init done

无法挂载镜像,有谁能帮助我吗

Labels (1)
0 Kudos
Reply
2 Replies

2,474 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello jianfei,

You need to burn the SD again or you have some issue with your memory try to run the DDR stress tool

https://community.nxp.com/docs/DOC-340179 

Regards

0 Kudos
Reply

2,474 Views
jianfeichang
Contributor IV

Hello Bio_TICFSL,

now SD is OK.

but galorce is error.I'm going to remove galcore from the file system,It is ok.When I insmod galcore.ko,The kernel hang.

It's kind of like this mistake,What am I supposed to do?QQ图片20191018134525.png

0 Kudos
Reply