i.MX 8M Mini: SPI-bus native CS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX 8M Mini: SPI-bus native CS

跳至解决方案
3,805 次查看
ristohedman
Contributor II

Hi,

I would like to ask NXP experts about SPI (ECSPI). My company is switching to iMX8 and in order to desighn the HW we need to know these details.

I've been studying 

     IMX8MMRM.pdf 

     8.1 External Signals and Pin Multiplexing

    10.1 Enhanced Configurable SPI (ECSPI) 

And asked my EVA- manufacturer but have not got an answer:

      How are SPI chip selects SS1, SS2 and SS3 muxed to hardware pins, (or balls or pads - which way ever one calls them) ?? 

      I heard that NXP is recommending to use gpio for chip selects (in Linux??) - is that true and if is, why?

Best Regards,

 

Risto H.

 

0 项奖励
回复
1 解答
3,772 次查看
ristohedman
Contributor II

Hi Yuri,

Finally an answer - not a good one for me but answer anyway.

BR, ristoH

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,799 次查看
Yuri
NXP Employee
NXP Employee

@ristohedman 
Hello,

   Customers can use Table 8-1 (Muxing Options) of the i.MX8Mm RM.
As for pin assignments - use section 5 (Package information and contact assignments)
of i.MX8Mm Datasheet.

https://www.nxp.com/docs/en/data-sheet/IMX8MMCEC.pdf

GPIO instead of "native" SS may be used for non supported modes, say for "long"
messages.

Regards,
Yuri.

0 项奖励
回复
3,793 次查看
ristohedman
Contributor II

Hi,

Hmmm, now I must have a great misunderstanding, if I try to search e.g. ECSPI1_SS1 in any 'mini'- related document, I can not find ??!!

 

br, ristoH

0 项奖励
回复
3,785 次查看
Yuri
NXP Employee
NXP Employee

@ristohedman 
Hello,

i.MX8Mm supports single eCSPI SS: ECSPI1_SS0 - there are no more (ECSPI1_SS1 ...).

https://community.nxp.com/t5/i-MX-Processors/How-can-I-use-ECSPI-SS1-2/m-p/848467

 

Regards,
Yuri.

0 项奖励
回复
3,773 次查看
ristohedman
Contributor II

Hi Yuri,

Finally an answer - not a good one for me but answer anyway.

BR, ristoH

0 项奖励
回复