i.MX 8 Mini cannot boot from Linux and not able to switch to Android

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8 Mini cannot boot from Linux and not able to switch to Android

Jump to solution
6,842 Views
littlebone
Contributor II

Hi all,

I flashed my i.MX8 Mini with the Linux image (L5.4.70_2.3.0_images_MX8MMEVK.zip) I downloaded from the official website and it worked well.

And then I tried to switch back to android image (android_p9.0.0_1.0.0-ga_image_8mmevk) also downloaded from the official website. But uuu is always blocked and keep repeating the "write -f u-boot-imx8mm-evk-uuu.imx -offset 0x57c00" step.

Since it does not work, I switched it back to Linux image again with the same image above. Though I can successfully flash the image, the board does not boot and looks like it is keeping reset again and again (The green D1 cpu and red D708 power LED goes off for a short instant every a few second).

Hopefully I could find some help here. Thank you.

Labels (2)
0 Kudos
Reply
1 Solution
6,816 Views
littlebone
Contributor II

Confirmed that the problem was caused by one wrong on/off setting on the switch. Thank you. 

View solution in original post

5 Replies
6,817 Views
littlebone
Contributor II

Confirmed that the problem was caused by one wrong on/off setting on the switch. Thank you. 

6,799 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Good news it works.

0 Kudos
Reply
6,830 Views
littlebone
Contributor II

BTW I am flashing the image with the instructions I found on NXP website (uuu.exe L4.14.78_1.0.0_ga_images_MX8MMEVK.zip and uuu.exe uuu-android-mx8mm-evk-sd.lst)

0 Kudos
Reply
6,830 Views
littlebone
Contributor II

Hi b45499,

Correct me if I am wrong, as I know the switch setting is the same for Android/Linux BSP before flashing/after flashed. That is, set to SDP mode before flashing and switch set to boot from eMMC mode after flashed. Thank you.

0 Kudos
Reply
6,830 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Have you set the right boot mode for your board to boot up? For linux and android download and boot up you can see our user guide, details in our documents.

 

0 Kudos
Reply