i.MX 6ULL - Is Qt5 Supported?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 6ULL - Is Qt5 Supported?

5,668 Views
brianptl
Contributor III

Hi All,

I am following the document "i.MX Yocto Project User's Guide.pdf".

I have set up the development environment, e.g.

$ mkdir imx-yocto-bsp
$ cd imx-yocto-bsp
m imx-4.9.88-2.0.0_ga.xml
$ repo sync

etc..

Once I have done this, I see a note in the document ~/imx-yocto-bsp/README-IMXBSP

Note Qt is not supported on i.MX 6UltraLite and i.MX 7Dual. It works on X11 backend only but is not a supported feature.

My questions are:

  • Does this note apply to the i.MX 6ULL? I think not from the wording, but I believe the 6ULL is based on the 6UL so I want to check.
  • Is there a matrix of supported software vs i.MX 6 variant that I can refer to in order to determine we are picking the correct chip for our software requirements?

Thanks,

Brian.

Labels (4)
3 Replies

5,030 Views
linda_zhang
Contributor IV

Hi Brian,

We have ported QT5.6.2 on our MYD-Y6ULX board, but imx6UL can not support GPU and hardware graphics.

It can only display from software but video effects might not too strong.

MEasy HMI QT Demo on i.MX6UL/6ULL MYD-Y6ULX Development Board - YouTube 

Best regards,

Linda

 

5,030 Views
ATAineri
Contributor III

And how to build yocto for imx6ull with qt5 and cross-compile qt application for it(or maybe better to compile it on the board)?

0 Kudos
Reply

5,028 Views
igorpadykov
NXP Employee
NXP Employee

Hi Brian

i.MX6ULL is reduced version of i.MX6UL and it is also not supported,

as described in sect.2.1 New features attached Release Notes:

Qt 5 is not supported for SoCs without hardware graphics. Qt 5 video is not supported on SoCs without a VPU.

i.MX Family Matrix

https://www.nxp.com/docs/en/brochure/FLYRIMXPRDCMPR.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply