i.MX 6ULL ADC usage

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX 6ULL ADC usage

跳至解决方案
1,423 次查看
sugiyamatoshihi
Contributor V

Hi, 

I have a question about how to use ADC of i.MX 6ULL.

When I checked IOMUXC_SW_MUX_CTL_PAD_GPIO1_IO01 register in Reference manual. There is no ADC selection in MUX_MODE.

Should it select GPIO1_IO01 ALT5 in MUX_MODE for ADC input?

Best Regards,

Sugiyama

标签 (1)
0 项奖励
回复
1 解答
1,277 次查看
art
NXP Employee
NXP Employee

There is no special IOMUX mode for the ADC input in the IOMUX Pad Configuration register since the ADC inputs are always connected to the corresponding pads. To minimize the possible signal contention and measurement error, the ADC input pad should be configured as GPIO (ALT5) input with no pull-up/pull-down/keeper circuit enabled.

Best Regards,

Artur

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,278 次查看
art
NXP Employee
NXP Employee

There is no special IOMUX mode for the ADC input in the IOMUX Pad Configuration register since the ADC inputs are always connected to the corresponding pads. To minimize the possible signal contention and measurement error, the ADC input pad should be configured as GPIO (ALT5) input with no pull-up/pull-down/keeper circuit enabled.

Best Regards,

Artur

0 项奖励
回复