i.MX 6ULL ADC usage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,403件の閲覧回数
sugiyamatoshihi
Contributor V

Hi, 

I have a question about how to use ADC of i.MX 6ULL.

When I checked IOMUXC_SW_MUX_CTL_PAD_GPIO1_IO01 register in Reference manual. There is no ADC selection in MUX_MODE.

Should it select GPIO1_IO01 ALT5 in MUX_MODE for ADC input?

Best Regards,

Sugiyama

ラベル(1)
0 件の賞賛
返信
1 解決策
1,257件の閲覧回数
art
NXP Employee
NXP Employee

There is no special IOMUX mode for the ADC input in the IOMUX Pad Configuration register since the ADC inputs are always connected to the corresponding pads. To minimize the possible signal contention and measurement error, the ADC input pad should be configured as GPIO (ALT5) input with no pull-up/pull-down/keeper circuit enabled.

Best Regards,

Artur

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,258件の閲覧回数
art
NXP Employee
NXP Employee

There is no special IOMUX mode for the ADC input in the IOMUX Pad Configuration register since the ADC inputs are always connected to the corresponding pads. To minimize the possible signal contention and measurement error, the ADC input pad should be configured as GPIO (ALT5) input with no pull-up/pull-down/keeper circuit enabled.

Best Regards,

Artur

0 件の賞賛
返信