i.MX 6 IPU interrupt control

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 6 IPU interrupt control

772 Views
sugiyamatoshihi
Contributor V

Hi, 

I have a question about IPUx_INT_CTLR_15 and IPUx_INT_STAT_15 register.

There is a bit DI0_CNT_EN_PRE_0_EN and DI0_CNT_EN_PRE_0 in 18th, but table 37-35 Functional Interrupts Summary sees like below.

pastedImage_1.png

Which name is correct?

What for this interrupt?

Best Regards,

Sugiyama

Labels (2)
0 Kudos
Reply
1 Reply

678 Views
b36401
NXP Employee
NXP Employee

Please refer chapter 37.5.20 Interrupt Control Register15 (IPUx_INT_CTRL_15) of i.MX 6Dual/6Quad Processor Reference Manual.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply