i.MX 6 DualLite Android 6 CANBus Send question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX 6 DualLite Android 6 CANBus Send question

1,015件の閲覧回数
ruei_chang
Contributor III

Hi all,

   Recently, we found CANBus has an issue on i.MX6 DualLite. We used the following links to implement CANBus function.

Here is the process of CANBus.

Flexcan/flexcan/frameworks/base/service/java/com/android/server at master · zhangjie201412/Flexcan ·... 

                                                ↓

Flexcan/com_android_server_FlexcanService.cpp at master · zhangjie201412/Flexcan · GitHub 

                                                ↓

Flexcan/flexcan.c at master · zhangjie201412/Flexcan · GitHub 

Now the issue happened in _flexcan_send  of flexcan.c When I call _flexcan_send this function frequently, it would return me an error. 

But if I had a delay for waiting 5ms of every  _flexcan_send), CANBus would be fine. It seems I couldn't call _flexcan_send too quick. 

Has anyone met this issue before?

It would be grateful if there is any solution to it.

I have highlighted the code which returned me an error.

static int _flexcan_send(struct flexcan_device_t* flexcan_device,int *data, int id, int dlc, int extended,int rtr, int infinite, int loopcount)
{
      int s = flexcan_device->s;
      struct can_frame frame;
      int i;
      int ret;
      for(i = 0; i < dlc; i++)
      {
         frame.data[i] = (char)data[i];
         // LOGI("[flexcan]--%d = %d .",i,data[i]);
         if(i == 8)
         break;
      }
      frame.can_id = id;
      frame.can_dlc = dlc;

      if (extended) {
         frame.can_id &= CAN_EFF_MASK;
         frame.can_id |= CAN_EFF_FLAG;
      } else {
         frame.can_id &= CAN_SFF_MASK;
      }

      if (rtr)
        frame.can_id |= CAN_RTR_FLAG;

      while (infinite || loopcount--) {
         ret = write(s, &frame, sizeof(frame));
         if (ret == -1) {
            perror("write");
            break;
         }
   }

   // close(s);
   return 0;
}

ラベル(1)
タグ(2)
0 件の賞賛
返信
0 返答(返信)