i.MA6SDL A1 pin.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,544件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6SDL package.

Please see Table 104 in IMX6SDLCEC Rev.4.

It mentions that A1 pin is removed from datasheet.

Then, I want to confirm whether solder ball on A1 pin is changend or not.

According to Figure 106 in IMX6SDLCEC Rev.3 and Figure 107 in IMX6SDLCEC Rev.4, there is no solder ball on A1 pin and it is not changed.

Is my understanding correct?

Best Regards,

Satoshi Shimoda

ラベル(2)
0 件の賞賛
返信
1 解決策
1,477件の閲覧回数
Yuri
NXP Employee
NXP Employee

   There is no solder ball on A1 location of the i.MX6 S/DL package,

and corresponding pin A1 is not connected to any i.MX6 S/DL internal

signal.


Have a great day,
Yuri.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,478件の閲覧回数
Yuri
NXP Employee
NXP Employee

   There is no solder ball on A1 location of the i.MX6 S/DL package,

and corresponding pin A1 is not connected to any i.MX6 S/DL internal

signal.


Have a great day,
Yuri.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信