IMX6 booting issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 booting issue

2,505件の閲覧回数
sureshkumarvavi
Contributor I

Hi,

I have one iMX6Q Saberlite Board without display. After the board is powered up, i am seeing an LED glowing on the board.

But i didnt see any trace on serial port (hyperterminal / minicom) to start the board.

I thinking some issue with bootloader(UBoot).

I have setted the pins in Normal Mode.I have set the proper buad rate and hardaware flow control settings.

Needed help in order to boot the board.

Regards,

Suresh

ラベル(1)
タグ(2)
0 件の賞賛
返信
3 返答(返信)

2,332件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Suresh

probably board is bricked, please look below

http://boundarydevices.com/unbricking-nitrogen6x-sabre-lite-i-mx6-board/

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,332件の閲覧回数
sureshkumarvavi
Contributor I

Hi igor,

Thanks for the quick response.

I tried with the link which you shared.

But i didnt see my device in 'lsusb' command.

Following is the trace which i got after connecting the board to pc using USB OTG.

Bus 002 Device 002: ID 8087:0024 Intel Corp. Integrated Rate Matching Hub

Bus 002 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub

Bus 001 Device 002: ID 8087:0024 Intel Corp. Integrated Rate Matching Hub

Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub

Is there anything else i need to install/configure  on my pc.

Regards,

Suresh

0 件の賞賛
返信

2,332件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Suresh

please post this on boundary devices forum

http://boundarydevices.com/support/

Best regards

igor

0 件の賞賛
返信