how to use flexCAN in imx6ull processor ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to use flexCAN in imx6ull processor ?

1,250 次查看
somnath_roy
Contributor I

hi all,

    i am using a SOM module by toradex it came with imx6ull processor 

i have changed the dtsi file and my module is loaded in startup. 

but i am getting a msg as 

[   13.641388] CAN device driver interface
[  OK  ] Reached target System Initialization.
[   13.677653] 2094000.can supply xceiver not found, using dummy regulator

and when i am using cansend utility i am not getting and signal in CAN_tx pin.

yet i am using can xceiver IC UJA1161 and my xceiver is powered up.

标签 (2)
0 项奖励
回复
1 回复

1,092 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Somnath

please connect other board or protocal analyzer and for testing

one can use unit tets (folder ..test/can) :
imx-test
www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复