how to set backlight pwms on imx6ull

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to set backlight pwms on imx6ull

2,410 Views
gokmenavci
Contributor II

i want to use a lcd and i need pwm signal 20 kHz

how can i use pwm on imx6ull evk ?

Labels (2)
Tags (2)
0 Kudos
Reply
2 Replies

2,189 Views
art
NXP Employee
NXP Employee

The Linux BSP already contains the PWM driver, refer to the Section 2.5 of the attached document for more information.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,189 Views
gokmenavci
Contributor II

yes, i checked the document. But i dont understand how i change the pwm period. the Linux BSP pwm period 200Hz but i need 20kHz for my LCD screen. How can i change it. In the document there is some software operation function. i dont know how to use these.

Any body can tell me ?

0 Kudos
Reply