how to resolve this can driver problem?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to resolve this can driver problem?

1,431 Views
pooja_todakar
Contributor I

hi,

i am interfacing CANFD to SPI driver in imx6ull processor

while sending data from CANFD board i m getting this error

~# ip link set can0 up type can bitrate 500000
[ 31.265249] IPv6: ADDRCONF(NETDEV_CHANGE): can0: link becomes ready
~ # ifconfig
can0 Link encap:UNSPEC HWaddr 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00
UP RUNNING NOARP MTU:16 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:10
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Interrupt:22

lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)

~ # cansend can0 123#aabbccdd
[ 938.791952] flexcan 2094000.flexcan can0: bus-off

and i m not receiving data,how resolve this one

Labels (1)
0 Kudos
Reply
1 Reply

1,372 Views
igorpadykov
NXP Employee
NXP Employee

Hi Pooja

one can look at examples of porting other spi driven peripheral drivers, like

How to use SPI slave within U-Boot? 

Porting small OLED display to i.MX6ULL 14x14 Evk 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply