how to reduce uboot time

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to reduce uboot time

1,097 Views
851931531
Contributor I

hi:

  I want to reduce boot time in i.mx8M mini, I fund the spl consume 0.8s,and the uboot consume 1s. so from power up to start kernel, consume about 1.8s. I have remove some boot_cmd that we do not  need in the config files,but it hasn't improved much.now my uboot.bin still have 400K.so wo want to how to  reduce uboot time?

   1 how to enable cache and mmu?

 2  how to set cpu freq is 1.8GHz?

Labels (1)
0 Kudos
Reply
1 Reply

1,021 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which version of BSP are you using?

0 Kudos
Reply