Alejandro,
Thank you for the pointer, I checked the URL and tried to identify the proper "defconfig" under "sources/meta-fsl-arm" folder and got:
meta-fsl-arm/recipes-kernel/linux/linux-timesys-3.0.15/defconfig
meta-fsl-arm/recipes-kernel/linux/linux-imx-3.10.9/mx6/defconfig
meta-fsl-arm/recipes-kernel/linux/linux-imx-2.6.35.3/imx28evk/defconfig
meta-fsl-arm/recipes-kernel/linux/linux-imx-2.6.35.3/mx5/defconfig
meta-fsl-arm/recipes-kernel/linux/linux-imx-2.6.35.3/imx23evk/defconfig
meta-fsl-arm/recipes-kernel/linux/linux-imx-3.0.35/mx6q/defconfig
meta-fsl-arm/recipes-kernel/linux/linux-imx-3.0.35/mx6dl/defconfig
meta-fsl-arm/recipes-kernel/linux/linux-imx-3.0.35/mx6sl/defconfig
meta-fsl-arm/recipes-kernel/linux/linux-imx-3.0.35/mx6s/defconfig
meta-fsl-arm/recipes-kernel/linux/linux-fslc/mxs/defconfig
meta-fsl-arm/recipes-kernel/linux/linux-fslc/defconfig
I am not sure which is the one for 3.10.17 version kernel on imx6q device? None of these defconfig files look like the one in build folder
520fc9c85e261a9959853268ecbe3d28 linux-imx/3.10.17-r0/defconfig
520fc9c85e261a9959853268ecbe3d28 linux-imx/3.10.17-r0/git/arch/arm/configs/imx_v7_defconfig
Does this mean that 3.10.17 version is not using any "defconfig" under "sources" folder?
Regards,
yanfeng