how to mux uart7(null modem)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to mux uart7(null modem)

2,408件の閲覧回数
wangjia
Contributor I

pinctrl_uart7: uart7grp {

                        fsl,pins = <

                              MX6UL_PAD_ENET2_RX_EN__UART7_DCE_TX     0x1b0b1

                              MX6UL_PAD_ENET2_TX_DATA0__UART7_DCE_RX  0x1b0b1

                        > ;

                };

 

configure like this , and disable the pinctrl_enet2  interface . but no TX our when

i am using the echo "test" >/dev/ttymxc6 .

 

but opposite the uart6 success like this configure :

pinctrl_uart6: uart6grp {

                        fsl,pins = <

                               MX6UL_PAD_ENET2_RX_DATA0__UART6_DCE_TX   0x1b0b1

                               MX6UL_PAD_ENET2_RX_DATA1__UART6_DCE_RX   0x1b0b1                            

                        > ;

                } ;

 

how can we enable the uart7  , anybody help me ?

Original Attachment has been moved to: imx6ul-14x14-evk.dts.zip

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,207件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi wang

one can check if enet2 is enabled in uboot (include/configs/mx6ul_14x14_evk.h)

with CONFIG_FEC_ENET_DEV == 1

and try to disable it too.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,207件の閲覧回数
wangjia
Contributor I

thanks you reply . Unfortunatly i has been disable it already .

because of no use of ENET2 .

#define CONFIG_FEC_ENET_DEV 0

#if (CONFIG_FEC_ENET_DEV == 0)

#define IMX_FEC_BASE                    ENET_BASE_ADDR

#define CONFIG_FEC_MXC_PHYADDR          0x2

#define CONFIG_FEC_XCV_TYPE             RMII

#elif (CONFIG_FEC_ENET_DEV == 1)

#define IMX_FEC_BASE                    ENET2_BASE_ADDR

#define CONFIG_FEC_MXC_PHYADDR          0x1  /* need board rework */

#define CONFIG_FEC_XCV_TYPE             RMII

#endif

0 件の賞賛
返信

2,207件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi wang

one can attach jtag or use memtool to check uart iomux registers,

CCM_CCGR uart clock gate and try manually write to UARTx_UTXD

Best regards

igor

0 件の賞賛
返信