how to modify u-boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to modify u-boot

5,861件の閲覧回数
梦田
Contributor II

Hello,

I am starting to use Yocto but I have a lots of difficulties to understand how it works.

This is the link:    file:///F:/freescale/QorIQ-SDK-V1.6-SOURCE-20140619-yocto/START_HERE.html

I just want to modify u-boot, how should I proceed ?

ラベル(1)
7 返答(返信)

4,825件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello 梦田,

Please refer to the application note QorIQ Linux SDK 1.6 Working With Yocto.

There is detailed description about how Yocto SDK 1.6 working, and the procedure to modify u-boot source or configuration and rebuild u-boot.

Please feel free to let me know for any confusion.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

4,825件の閲覧回数
梦田
Contributor II

It says"

Modify U-Boot configuration.

  1. $ modify UBOOT_MACHINESValues for UBOOT_MACHINES are listed in meta-fsl-ppc/conf/machine/<machine>.confe.g.UBOOT_MACHINES = "P1023RDB"

"

0 件の賞賛
返信

4,825件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello 梦田,

Thanks. It's a mistake, I will correct it, it should be

  1. Modify UBOOT_MACHINES variable in meta-fsl-ppc/conf/machine/<machine>.conf, for example meta-fsl-ppc/conf/machine/p1023rdb.conf, you could use "vi" to open and edit the conf file.

Thanks,

Yiping

0 件の賞賛
返信

4,825件の閲覧回数
梦田
Contributor II

Hello Yiping Wang,

     I just find another question. When I begin to configure the Linux Kernel, I should update KERNEL_DEFCONFIG variable in meta-fsl-ppc/conf/machine/t4240qds.conf and update KERNEL_DEVICETREE variable in meta-fsl-ppc/conf/machine/t4240qds.conf.

     But I cannot understand how can I update them.


     Thanks,

    mengtian

0 件の賞賛
返信

4,825件の閲覧回数
梦田
Contributor II

Hello Yiping Wang,

     Thank you for your answer sincerely.

0 件の賞賛
返信

4,825件の閲覧回数
梦田
Contributor II

Dear Yiping Wang,

Thanking for your answer so much.

I just follow the web station,but when I follow this step,I came across problems.

It says"

Modify U-Boot configuration.

  1. $ modify UBOOT_MACHINESValues for UBOOT_MACHINES are listed in meta-fsl-ppc/conf/machine/<machine>.confe.g. UBOOT_MACHINES = "P1023RDB"

"

but I cannot find the command of “modify”, could you help me?

(ps:Could I ask questions in Chinese on this web station?)

                                                                                 Thank you,

                                                                                   mengtian

0 件の賞賛
返信

4,825件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please forward this request to PowerQUICC Processors

QorIQ Processors

~Yuri.

0 件の賞賛
返信